{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Deployment of Data Center Expert 7.9.x VM only allows up to 8 CPU cores.

Issue:
Deployment of Data Center Expert 7.9.x only allows up to 8 CPU cores.

Product Line:
Data Center Expert

Environment:
DCE potentially any version
AP94VMACT deployment on VMware ESXI

Cause:
Data Center Expert VM was only built with the maximum capacity of 8 CPU cores. This was due to compatibility with ESXI version 4.

Resolution:
This can be edited in VMware and changed to allow more cores.

Shut the vm down.
Right click the VM in vsphere.
Go to Compatibility --> Upgrade Compatibility
conmpatibility_menu.PNG

You will get a warning stating that this is an irreversible operation. Hit yes.
compatibility_warning.PNG

Choose the last one in the "Compatible With" list and hit OK
compatible_with.PNG

You should now be able to set over 8 CPUs for the DCE 7.9.2
compatible_edit_settings.PNG



***Please note that if you have deployed a version and increased the number of cores, then upgraded that version to the next (not a fresh VM deployment), you will not see this issue.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: