{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I use the READ_DDT function block to configure read messages for the BMENUA0100 communication module?
Issue:
Configuring the READ_DDT to read the BMENUA0100 module's information


Product Line:
BMENUA0100, EcoStruxure Control Expert


Resolution:
Below is a sample code on how to configured the READ_DDT function block
image2

image1

Below is a sample code using the READ_DDT function block to read messages from the BMENUA0100 communication module.
Note: Ensure that the RECP_DDT variable has the data type "T_BMENUA0100" DDT

image3

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: