{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can't I download to a brand new HMIGTO / HMIGK with Vijeo Designer 6.2 SP11 or older?
Issue:
Can't download to a new HMIGTO / HMIGK using Vijeo Designer v6.2 SP11 or older.

Product Line:
HMIGTO and HMIGK families of HMIs

Environment:
Vijeo Designer v6.2

Cause:
The new HMIGTO/HMIGK families have a hardware component change that requires Vijeo Designer v6.2 SP12.

Resolution:
The Harmony HMIGTO and HMIGK families of HMIs that are manufactured recently withSV4.0 or later on the sticker on the back of the HMI require Vijeo Designer v6.2 Service Pack 12.

Please find the download links for SP12 here:
https://www.se.com/us/en/faqs/FAQ000239885/

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: