{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If using NetBotz rest API, Pod Enclosure Number (podEncNum) may be either 0 or 1 based
Issue:
If using NetBotz rest API, Pod Enclosure Number (podEncNum) may be either 0 or 1 based

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755

Cause:
There are 2 different numbering systems in the NetBotz code, some are 0 based while others are 1 based.
This is exposed in the podEncNum field that we expose in our REST API, mass config, SNMP, Modbus.

Resolution:
For the 150 and 155 pod’s the podEncNum values will be 0-based
For the 170 anad 175 pod’s the podEncNum values will be 1-based
For the AP9520TH the podEncNum values will be 0-based
NOTE that the numbers allocated are distinct across the three sequences based on enclosure type / pod model.

Schneider Electric Egypt and North East Africa

If using NetBotz rest API, Pod Enclosure Number (podEncNum) may be either 0 or 1 based
Issue:
If using NetBotz rest API, Pod Enclosure Number (podEncNum) may be either 0 or 1 based

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755

Cause:
There are 2 different numbering systems in the NetBotz code, some are 0 based while others are 1 based.
This is exposed in the podEncNum field that we expose in our REST API, mass config, SNMP, Modbus.

Resolution:
For the 150 and 155 pod’s the podEncNum values will be 0-based
For the 170 anad 175 pod’s the podEncNum values will be 1-based
For the AP9520TH the podEncNum values will be 0-based
NOTE that the numbers allocated are distinct across the three sequences based on enclosure type / pod model.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top