{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which virtual environment is EcoStruxure Control Expert V15.3 supported on?
Issue:
Supported virtual environment for EcoStruxure Control Expert V15.3


Product Line:
EcoStruxure Control Expert


Resolution:
Control Expert V15.3 has been successfully tested in the following Virtual environment:
• VMware vSphere –Hypervisor- ESXi
• VMware Workstation 15.5.2
• Oracle VirtualBox 6.1.0

Note: It has not been tested on Virtual Box 5.2.16-123759
Note: The amount of RAM of host computer needs to be 16 GB if Control Expert is used in a Virtual machine with 8 GB assigned to the Virtual machine

Schneider Electric Egypt and North East Africa