Control Expert 15.0 SP1 reports Fatal error when upgrading M340 firmware from V2.40 to V2.70..
The validated workaround is
• Open STA file
• Export application as ZEF file
• Open this ZEF file
• Perform the replace CPU from V2.40 to V2.70 (no errors because COBID not yet performed)
• Rebuild the application
• Save STA – new STA is with V2.70 CPU
Released for:Schneider Electric Egypt and North East Africa