{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a PBPQOU4A100CEGL630 compatible with part number PBPQOU4A100CEGL630T

Issue:

Checking compatibility

Product Line:

Busway

Environment:

PBPQOU4A100CEGL630

Cause:

N/A

Resolution:

Both part numbers are the same with the exception of the T suffix, which is just the addition of a carry handle option.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: