{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many WebViewer connections are supported in EcoStruxure Operator Terminal Expert at one time?
Issue
How many simultaneous WebViewer browsing instances are supported in EcoStruxure Operator Terminal Expert for the HMIST6, HMISTM6, and iPCs?

Product Line
EcoStruxure Operator Terminal Expert v3.3 and up

Resolution
The maximum simultaneous client connections from a browser to an HMI running EcoStruxure Operator Terminal Expert v3.3 and up is as follows:
HMIST6 and HMISTM6 Series: 3
iPC models running EcoStruxure Operator Terminal Expert Runtime: 5

This information can be found in the Feature Guide launched from EcoStruxure Operator Terminal Expert v3.3 and up from the help "Help" dropdown menu.
Section: Configuring the System > Data Access (Remote Operation) Settings > Using EcoStruxure Operator Terminal Expert Web Viewer > EcoStruxure Opreator Terminal Expert Web Viewer Overview and Development Workflow
EcoStruxure Operator Terminal Expert Feature Guide - Web Viewer section

Schneider Electric Egypt and North East Africa