{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to disable weak ciphers in KVM2132P, KVM2116P, and KVM1116P?
Product Line: KVM2132P, KVM2116P, and KVM1116P

Environment: KVM Switches

Cause: Weak ciphers in KVM switches.

Resolution:
1. Log in to the KVM's web management console and go to Maintenance->Terminal.
KVM-terminal
2. On the terminal window, issue the following commands to disable the weak ciphers:
enabletlsv1.0 0
enabletlsv1.1 0
enablerc4 0
setsslcipher 2

KVM-terminal-tls

KVM-terminal-rc4
3. Each command should provide an output confirming if it is successfully carried out. Issuing the 'get' command shows which ciphers are used by the KVM along with the other statuses.
Here is the description of the commands used:
  • enabletlsv1.0 0 - Disables TLS 1.0
  • enabletlsv1.1 0 - Disables TLS 1.1
  • enablerc4 0 - Disables RC4
  • setsslcipher 2 - Disables DES, 3DES, and sets the cipher strength.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: