{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the ETH STS flash patterns for the M340?

The ETH STS should either be on Solid indicating Communications OK or a pattern of flashing/pause/flashing. If it is off this would indicate a hardware issue.

Below are the flash pattern descriptions.

2 flashes - Invalid MAC address

3 flashes - No link; Incorrect/no cable connected or no valid device at the other end of the cable.

4 flashes - Duplicate Ip address; Make sure that you did not inadvertently set the PC/Laptop to the M340 address.

5 flashes - Waiting for a Served IP address; Either the switch on the back is set for Boot P or the project is configured for 'From a Server' and nothing is serving.

6 flashes - Default Ip; This probably means that the switch on the back is set to Clear IP or Disabled. No Ip address has been assigned. https://www.se.com/us/en/faqs/FA213636/

7 flashes- Probably means that the switch is set to Stored but the projects Eth network was not bound to the Ethernet port. (or any other Rotary Switch/Internal config conflict) https://www.se.com/us/en/faqs/FA233493/

Schneider Electric Egypt and North East Africa