Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Control Expert V15.3 CANopen DTM warning

Issue

When opening Control Expert v15.3 and the DTMs update it returns: “Warning: 0_2CANopenComm.USB_to_CANopenC000.1: DTMCatalogBuilder: AddDTMInfoToCatalog failed!”

 

Resolution

Uninstall the CXM DTM from add/remove programs then run setup.exe from the CXM Gateway DTM folder that is part of the v15.3 installation files (iso).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: