Search FAQs
FDM128 automatic device discovery issue of IFM Micrologic (Compact NS/Compact NSX) via PaS600
Issue
The FDM128 automatic device discovery issue of IFM Micrologic (Compact NS/Compact NSX) via PaS600 architecture. Randomly missing of slave devices while discovering.
Product Line
FDM128
PAS600
IFM
Micrologic (Compact NS + Compact NSX)
Environment
FDM128 v8.0.30
PAS600 FW1.6.0/1.5.1
Micrologic (Compact NS + Compact NSX) via IFM
Cause
It is identified that due to synchronization problem, the device is randomly missing some of the slave ids during discovery.
Resolution
A temporary suggested solution is that the user can discover the missed slave IDs in the following way.
![img1 img1](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFN9QAN&oid=00DA0000000abSmMAI)
![img2 img2](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNAQA3&oid=00DA0000000abSmMAI)
![img3 img3](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNBQA3&oid=00DA0000000abSmMAI)
Slave ID 4 is missing.
![img4 img4](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNCQA3&oid=00DA0000000abSmMAI)
![img5 img5](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNDQA3&oid=00DA0000000abSmMAI)
![img6 img6](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNTQA3&oid=00DA0000000abSmMAI)
![img7 img7](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNUQA3&oid=00DA0000000abSmMAI)
![img8 img8](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNVQA3&oid=00DA0000000abSmMAI)
![img9 img9](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNWQA3&oid=00DA0000000abSmMAI)
![img10 img10](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNXQA3&oid=00DA0000000abSmMAI)
![img11 img11](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DhFNYQA3&oid=00DA0000000abSmMAI)
Note
This issue will be fixed in next FW release of FDM128.
The FDM128 automatic device discovery issue of IFM Micrologic (Compact NS/Compact NSX) via PaS600 architecture. Randomly missing of slave devices while discovering.
Product Line
FDM128
PAS600
IFM
Micrologic (Compact NS + Compact NSX)
Environment
FDM128 v8.0.30
PAS600 FW1.6.0/1.5.1
Micrologic (Compact NS + Compact NSX) via IFM
Cause
It is identified that due to synchronization problem, the device is randomly missing some of the slave ids during discovery.
Resolution
A temporary suggested solution is that the user can discover the missed slave IDs in the following way.
- Discover the slaves connected from slave ID 1-6
- Click on Start and Discovery process will be in progress. List of Discovered devices given below.
Slave ID 4 is missing.
- Tick the selection boxes and press OK
- Give Yes
- Give the slave ID of the missed slave or select a range in which missed one should be included and click on start
- Missed device will get discovered. Tick the selection and press OK
- Give No for connecting additional Modbus serial line devices
- All Devices from slave ID 1-6 are discovered.
- General view
Note
This issue will be fixed in next FW release of FDM128.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: