{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Ecostructure Machine SCADA Expert, Is it possible to work alarms in Excel and then import the alarms.

Issue:

Is it possible to work alarms in Excel and then import the alarms in EcoStruxure Machine SCADA Expert.

Product Line:

EcoStruxure Machine SCADA Expert (all versions)

Resolution:

There is no export/import option that would allow you to work the Alarms sheet outside of EcoStruxure Machine SCADA Expert.

But there is a workaround that can be used:

In Machine SCADA Expert:

Create or open the Alarms sheet.

Add a few alarms to it to have some examples of each types of alarms to be created.

With the mouse, select all the alarms in the sheet and do a copy. (CTRL-C or right click - Copy)

Open Excel and paste all the alarms of the sheet into a spreadsheet. (CTRL-V or right click - Paste)

Modify the spreadsheet to add or modify the alarms.

Once the modifications done. Select all the alarms in the spreadsheet and copy/paste in the Alarms sheet of Machine SCADA Expert.

Notes:

If some tag names do not exist in Machine SCADA Expert, there will be a prompt asking to create them.

This workaround will have to be used for each Alarms sheets of the Machine SCADA Expert project.

Sometime, the shortcuts CTRL-C and CTRL-V do not work in Machine SCADA Expert. Use the right click button in this situation.

Schneider Electric Egypt and North East Africa