{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the current generated for a channel on the BMXAMO0410 for a 10VDC signal?

Issue
I am trying to determine voltage drop from a 2-10VDC signal generated by a BMXAMO0410 AO Module.
What is the current generated at the device to provide the 10VDC signal?

Product Line
X80 Analog I/O Modules - BMXAMO0410

Environment
Electrical characteristics

Resolution
For the BMXAMO0410, per channel, the minimum load impedance for voltage output is 1 kOhm. 
Where the min load impedance is 1 kOhm, that means at +10VDC, the max current draw cannot exceed 10mA. 10vdc/1000 ohm= 10mA

Also see: https://en.wikipedia.org/wiki/Output_impedance

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.