{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
EcoStruxure Control Expert - Error: CRA Drop tool is missing in the CPU DTM device list

Product line
EcoStruxure Control Expert

Issue
When you update a project from Unity Pro 13 to Control Expert 15 you may receive these errors:

The CRA Entry <drop number = [1] name = CRA_NAME> of the <Ethernet Network Manager> tool is missing in the CPU DTM device list.
The CRA <drop number = [1]name = CRA_NAME> of the Configuration EIO bus is missing in the CPU DTM device list.
ERROR: The application has been corrupted. The configuration of the EIO CRAs is inconsistent comparing the different parts of the application. See previous message(s)
Machine generated alternative text: Import File  (Network_491 : [MAS [ - :  (Channel (0.0.0 ) RIODlOBML2)  (Channel (0.0.O ) RIODlOBML2)  (Channel (0.0.0 ) RIODlOBML2)  (Channel (0.0.0 ) RIODlOBML2)  (Channel (0.00 ) RIODIOBML?)  (Channel (0.0.0 ) RIODlOBML2)  (Channel (0.0.O ) RIODlOBML2)  Process failed : 15 Error(s). 3 Warning(s)  Ethemet N  O error(s). 0 warning(s)  The CRA entry <drop number = [1] name = of the (Ethernet Network Manager) tool is missing in the CPU DTM device list  The CRA entry (drop number = [2] name = of the (Ethernet Network Manager) tool is missing in the CPU DTM device list  The CRA entry (drop number = 13] name = of the (Ethernet Network Manager) tool is missing in the CPU DTM device list.  The CRA (drop number - [11 name of the Conngurauon Elo bus is missing in the CPU DTM device list.  The CRA <drop number - name - 140CRA_OO?) of the Configuration El() bus is missing in the CPU DTM device list.  The CRA <drop number = [31 name = of the Configuration EIO bus is missing in the CPU DTM device list.  ERROR: The application has been corrupted. The contiguratjon ot the EIO CRAS is inconsistent comparing the ditterent parts of the application. See previous message(s).

Resolution
The workaround for this error is changing the CPU firmware version on Control Expert to update the DTM, then you should be able to compile without error.

Schneider Electric Egypt and North East Africa