Search FAQs
Do you need a special DTM file to connect Somove to the ATV650F or floor standing Drives?
Issue:
Connecting Somove to the ATV650 floor standing drives.
Product Line:
ATV630F and ATV650F or Floor Standing Version ATV630 or ATV650.
Environment:
All
Cause:
DTM software for Somove to connect to the ATV650 Floor standing drives.
Resolution:
The standard ATV600 DTM will include the option for the ATV630 and ATV650 floor standing drives.
Altivar Process ATV6xx DTM Library DTM files | Schneider Electric (se.com)
Example below:
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: