undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Runtime Calibration Refused due to UPS in invalid State

Issue:
My NMC show Runtime Calibration Refused due to UPS in invalid State when attempting to run a Calbration test on my SRTG UPS

Product Line:
Smart-UPS SRTG

Environment:
All models, All Serial Numbers

Cause:
The SRTG range of UPS do not have a runtime calibration test like the SRT range do,  the NMC firmware is shared by the SRT and SRTG UPS which is why the option is showing.

A manual calibration test must be performed by removing AC power from the UPS and letting the battery power the UPS until it is discharged, and then AC power introduced again to charge the batteries.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: