Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Easy UPS Online software (Schneider UPS/APC UPS) has been discontinued

Product Line: 

Schneider UPS Software 


Environment:

Any SRV UPS with APV9601/ APVS9601 installed using Schneider UPS software

 

Cause:

APV9601/ APVS9601 is discontinued.

 

Resolution:

The Easy UPS Online SNMP Cards (APV9601, APVS9601) are discontinued as of 31st Aug 2023.

In line with the SNMP Cards, the Easy UPS Online Software & the Shutdown Wizard are discontinued too. Please note that SRV UPS are supported with PowerChute Serial Shutdown for Serial/USB communication and AP9544 along with PowerChute Network Shutdown for network communication, hence there's no dependency on this software.


If the users wish to continue using their APV9601/APVS9601 and needs to use the associated UPS monitoring software &/or shutdown wizard, the last version of the software and firmware update file for APV9601/APVS9601 can be downloaded from this FAQ.

Please be advised that we will no longer publish any updates or provide support because the software is now discontinued.

Schneider Electric Egypt and North East Africa

Attachment(s)
installAPCUPS_windows.zip [332.28 MB]
2687-02S1.s19.zip [345.33 KB]
Easy UPS Online Monitoring Software v2.6-GA-01-23248 Release Notes.pdf [74.28 KB]
ShutdownWizard_APC.zip [51.77 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: