Search FAQs
Can I use Modbus RTU in TCP/UDP with RemoteConnect to communicate to remote SCADAPack x70 devices?
In certain circumstances a user may wish to use Modbus RTU in/over UDP protocol to communicate to remote x70 devices over a cellular network or serial to ethernet gateway. Currently there is no option for this in RemoteConnect.
The options for the PC communications DTM are listed below:
DNP3 USB
DNP3 Serial*
DNP3/TCP
DNP3/UDP
Modbus/TCP USB
Modbus RTU*
Modbus/TCP
* If using a serial connection, the logic editor is not avialeble as the logic editor requires a TCP/IP connection
These are accessed via the PC Communication Settings - SCADAPack CommDTM
![PCComm Settings PCComm Settings](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000BYRL3QAP&oid=00DA0000000abSmMAI)
The options for the PC communications DTM are listed below:
DNP3 USB
DNP3 Serial*
DNP3/TCP
DNP3/UDP
Modbus/TCP USB
Modbus RTU*
Modbus/TCP
* If using a serial connection, the logic editor is not avialeble as the logic editor requires a TCP/IP connection
These are accessed via the PC Communication Settings - SCADAPack CommDTM
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: