Search FAQs
How to set sensitivity for BVX series 700VA , 900VA, 1200VA, 1600VA, 2200VA?
Issue:
How to set sensitivity for BVX series?
Product Line:
Back-UPS models beginning with BVX
Environment:
All models specified above, All Serial Numbers
Cause:
There are times that the sensitivity settings need to be changed due to the actual condition of the main source/utility in order to keep the UPS operation smooth and normal.
Resolution:
Voltage Sensitivity Adjustment
How to set sensitivity for BVX series?
Product Line:
Back-UPS models beginning with BVX
Environment:
All models specified above, All Serial Numbers
Cause:
There are times that the sensitivity settings need to be changed due to the actual condition of the main source/utility in order to keep the UPS operation smooth and normal.
Resolution:
Voltage Sensitivity Adjustment
Press and hold the power On/Off button for 10 seconds until a beep is heard. The LED will flash and sensitivity LOW is set.
If press and hold the power On/Off button for 10 seconds again, the LED will be On and sensitivity MEDIUM is set.
If press and hold the power On/Off button for 10 seconds again, the LED will be On and sensitivity MEDIUM is set.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Explore more
Product: