Search FAQs
How to update M580 CPU NTP time via BMENOC0321 module
It is possible to update the cpu time from the NTP time provided by the BMENOC0321 MODule installed on the same rack. This is not done automatically, and we need to program It:
1- Enable the "Network Time Service" on the DTM of the BMENOC0321:
![BMENOC0321 DTM BMENOC0321 DTM](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000C6JvPQAV&oid=00DA0000000abSmMAI)
2- Open the "Network Time Service " in the service list and put the NTP remote server IP address. You can customise the Polling period, the Time Zone option, etc:
![Network Time Service configuration Network Time Service configuration](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000C6JvQQAV&oid=00DA0000000abSmMAI)
3- Import the attached program section in your program:
![Import section Import section](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000C6KBiQAN&oid=00DA0000000abSmMAI)
4- Configure the DFB by putting the module rack position and its IP address:
![DFB configuration DFB configuration](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000C6KBjQAN&oid=00DA0000000abSmMAI)
5- Use the "Enable" pin to activate the DFB and the Sync_PLC to enable the time synchronization.
6- Enable "Dynamic Arrays" variables in the project settings:
![Project settings Project settings](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000C6KBkQAN&oid=00DA0000000abSmMAI)
The CPU time will be updated after enabling the DFB:
![Animated DFB Animated DFB](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000C6KBlQAN&oid=00DA0000000abSmMAI)
PS: No need to enable the "NTP client" service of the CPU.
1- Enable the "Network Time Service" on the DTM of the BMENOC0321:
2- Open the "Network Time Service " in the service list and put the NTP remote server IP address. You can customise the Polling period, the Time Zone option, etc:
3- Import the attached program section in your program:
4- Configure the DFB by putting the module rack position and its IP address:
5- Use the "Enable" pin to activate the DFB and the Sync_PLC to enable the time synchronization.
6- Enable "Dynamic Arrays" variables in the project settings:
The CPU time will be updated after enabling the DFB:
PS: No need to enable the "NTP client" service of the CPU.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Product:
Explore more
Product: