Search FAQs
Access to SC&LV maintenance webserver using http://192.168.10.10
Answer:
This access is used for example when changing module's IP address or upgrading firmware.
Always make sure that the module's Ethernet connection is isolated from other modules
Still it may not be possible to ping or to connect to http://192.168.10.10 if there has been an IP@ conflict issue.
Please set your Laptop IP as 192.168.10.11
Note also that this access may be disabled during commissioning through T300 webserver as an hardening measure.
Use also T300 webserver to reenable it when relevant for maintenance purpose.
Connect now with http://192.168.10.10
This access is used for example when changing module's IP address or upgrading firmware.
Always make sure that the module's Ethernet connection is isolated from other modules
Still it may not be possible to ping or to connect to http://192.168.10.10 if there has been an IP@ conflict issue.
Please set your Laptop IP as 192.168.10.11
- Well think to shut down/on the module AFTER having disconnected the Ethernet connections
Note also that this access may be disabled during commissioning through T300 webserver as an hardening measure.
Use also T300 webserver to reenable it when relevant for maintenance purpose.
Connect now with http://192.168.10.10
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: