Search FAQs
How to download CPU OS Quantum using Modbus Plus protocol?
Context
The download of the Quantum CPU operating system can only be done through a direct connection between the PC and the CPU using the Modbus or Modbus Plus protocol.
However Modbus Plus communication is faster than Modbus communication and requires less time to download a binary file.
Prerequisites
Adresse du processeur Modbus Plus
On Modbus Plus, the default CPU address is address 1.
NOTE: Verify that the Modbus or Modbus Plus 1 address is not used by any device other than the CPU on the network. If another device uses address 1, change it to an address not used on the network.
Installing the Modbus Plus communication adapter
To install the Modbus Plus Communication Adapter (TSXCUSBMBP) hardware, complete the following steps :
To modify the Modbus Plus address of the TSXCUSBMBP adapter:
Open Start → All Programs → Schneider Electric - MBX Driver Suite → Setup → MBX Device Drivers.
Select the TSXCUSBMBP adapter and click Modify.
When prompted, select Launch Device Manager.
In Device Manager, select the USB adapter under Modicon Network MBX Devices → USB TSXCUSBMBP
In the configuration window, select the Device Settings tab.
In the Node Address field, select an address value: 2 for example (the address of the TSXCUSBMBP adapter must be different from the address of the CPU).
The Modbus Plus address of the TSXCUSBMBP adapter is now defined.
The TSXCUSBMBP adapter is ready to be used for updating a CPU module.
Product Line
CPU Quantum, TSXCUSBMBP,
Environment
Windows 10 Pro, OS Loader, Modbus Plus Driver Suite
The download of the Quantum CPU operating system can only be done through a direct connection between the PC and the CPU using the Modbus or Modbus Plus protocol.
However Modbus Plus communication is faster than Modbus communication and requires less time to download a binary file.
Prerequisites
- The Modbus Plus Driver software must already be installed on the PC because it is the driver which will allow the PC to recognize the TSXCUSBMBP cable
- OS Loader must also be installed on the PC because it is the software that allows the OS to be transferred to the PLC
- TSXCUSBMBP Modbus Plus USB adapter which is the Modbus Plus interface on the PC
Adresse du processeur Modbus Plus
On Modbus Plus, the default CPU address is address 1.
NOTE: Verify that the Modbus or Modbus Plus 1 address is not used by any device other than the CPU on the network. If another device uses address 1, change it to an address not used on the network.
Installing the Modbus Plus communication adapter
To install the Modbus Plus Communication Adapter (TSXCUSBMBP) hardware, complete the following steps :
- Connect the TSXCUSBMBP adapter to a USB port on your computer.
- Follow the installation process until a message appears indicating that the new hardware is ready for use.
- Restart your computer.
- Define the Modbus Plus address of the TSXCUSBMBP adapter.
To modify the Modbus Plus address of the TSXCUSBMBP adapter:
Open Start → All Programs → Schneider Electric - MBX Driver Suite → Setup → MBX Device Drivers.
Select the TSXCUSBMBP adapter and click Modify.
When prompted, select Launch Device Manager.
In Device Manager, select the USB adapter under Modicon Network MBX Devices → USB TSXCUSBMBP
In the configuration window, select the Device Settings tab.
In the Node Address field, select an address value: 2 for example (the address of the TSXCUSBMBP adapter must be different from the address of the CPU).
The Modbus Plus address of the TSXCUSBMBP adapter is now defined.
The TSXCUSBMBP adapter is ready to be used for updating a CPU module.
- Connect the Modbus Plus adapter cable between the TSXCUSBMBP and the CPU.
- Selection of the IOS loading operation on the device
- Choice of communication driver
- Selection of the target equipment by entering its target address and connection
- Final comparison between OS to download and the OS in the equipment
- Loading the OS on the equipment
- Confirmation of the transfer of the OS to the equipment
- Transfer in progress
Product Line
CPU Quantum, TSXCUSBMBP,
Environment
Windows 10 Pro, OS Loader, Modbus Plus Driver Suite
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Explore more
Product: