Search FAQs
V321 and IO unit maintenance LED on
Issue
Customer found that every now and then the maintenance LED on V321 and I/O unit is on and off.
_____________________________________________________________
Product Line
VAMP321
_____________________________________________________________
Environment
All firmware version
_____________________________________________________________
Root Cause
Please check if the address of VAM4C is 32 or not.
As stated in our manual, address 32 is reserved for Master Unit, and only one device can be set to Master mode in one Arc system, if two masters exist in same Arc system, it will cause some errors in system.
![1 1](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000EUhxcQAD&oid=00DA0000000abSmMAI)
![2 2](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000EUhxdQAD&oid=00DA0000000abSmMAI)
_____________________________________________________________
Solution
Set the address of VAM4C to another address except 32 and install the system again.
![3 3](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000EUhxeQAD&oid=00DA0000000abSmMAI)
Customer found that every now and then the maintenance LED on V321 and I/O unit is on and off.
_____________________________________________________________
Product Line
VAMP321
_____________________________________________________________
Environment
All firmware version
_____________________________________________________________
Root Cause
Please check if the address of VAM4C is 32 or not.
As stated in our manual, address 32 is reserved for Master Unit, and only one device can be set to Master mode in one Arc system, if two masters exist in same Arc system, it will cause some errors in system.
_____________________________________________________________
Solution
Set the address of VAM4C to another address except 32 and install the system again.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: