{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a Model 6 MCC be configured to 415VAC 50Hz voltage system?

415v 50hz is available for Model 6 MCC's as a special. We can issue special pricing for the application. Will have to know if there are any control power transformers or power supplies that will need to be converted.

Schneider Electric Egypt and North East Africa