Search FAQs
What are the basic troubleshooting steps for the Back-UPS Pro BR/BN "MS/MS2/M2/M2-CA" models?
Issue:
What are the basic troubleshooting steps for the Back-UPS Pro BR/BN "MS/MS2/M2/M2-CA" models?
Product Line:
APC Back-UPS Pro BR 1000/1350/1500 MS/MS2
APC Back-UPS Pro BN 1100/1350/1375/1400/1500 M2
APC Back-UPS Pro BN BN 1100/1350/1500 M2-CA
Environment:
All Serial Numbers
Cause:
During normal operation, you may find your UPS not functioning as expected. This may be due to a malfunction, configuration issue, or the install environment.
This document will assist you with basic troubleshooting steps.
Resolution:
What are the basic troubleshooting steps for the Back-UPS Pro BR/BN "MS/MS2/M2/M2-CA" models?
Product Line:
APC Back-UPS Pro BR 1000/1350/1500 MS/MS2
APC Back-UPS Pro BN 1100/1350/1375/1400/1500 M2
APC Back-UPS Pro BN BN 1100/1350/1500 M2-CA
Environment:
All Serial Numbers
Cause:
During normal operation, you may find your UPS not functioning as expected. This may be due to a malfunction, configuration issue, or the install environment.
This document will assist you with basic troubleshooting steps.
Resolution:
Problem | Possible Cause | Corrective Action |
Back-UPS will not switch on. | The Back-UPS is not connected to AC power. | Ensure that the Back-UPS is securely connected to an AC outlet. |
The circuit breaker has been tripped. | Disconnect non-essential equipment from the Back-UPS. Reset the circuit breaker. Re-connect equipment one item at a time. If the circuit breaker is tripped again, disconnect the device that caused the trip. | |
The internal battery is not connected. | Connect the battery | |
The AC input voltage is out of range | Adjust the transfer voltage and sensitivity range. | |
The Back-UPS does not provide power during a AC power outage. | Ensure that essential equipment is not plugged into a SURGE ONLY outlet. | Disconnect equipment from the SURGE ONLY outlet and re-connect to a Battery Backup outlet. |
The Back-UPS is operating on battery power, while connected to AC power. | The plug has partially pulled out of the wall outlet, the wall outlet is no longer receiving AC power, or the circuit breaker has been tripped. | Ensure that the plug is fully inserted into the wall outlet. Ensure that the wall outlet is receiving AC power by checking it with another device. |
The Back-UPS is performing an automatic self test. | No action is necessary. | |
The AC input voltage is out of range, the frequency is out of range, or the waveform is distorted. | Adjust the transfer voltage and sensitivity range. | |
The Back-UPS does not provide the expected amount of backup time. | Battery Backup outlets may be fully or improperly loaded. | Disconnect non-essential equipment from the Battery Backup outlets and connect the equipment to SURGE outlets. |
The battery was recently discharged due to a power outage and has not fully recharged. | Charge the battery cartridge for 16 hours. | |
The battery has reached the end of its useful life. | Replace the battery | |
The REPLACE BATTERY indicator is illuminated | The battery has reached the end of its useful life. | Replace the battery as early as possible |
The OVERLOAD indicator is illuminated. | The equipment connected to the Back-UPS is drawing more power than the Back-UPS can provide. | Disconnect non-essential equipment from the Battery Backup outlets and connect the equipment to SURGE outlets. |
The SYSTEM ERROR indicator is illuminated, all the front panel indicators are flashing. | There is an internal error | Determine which internal error message is displayed by matching the number displayed on the LCD with the corresponding Error Message (see "System Errors") and contact SEIT Technical Support. |
System Errors | F01 On-Battery Overload | Turn the Back-UPS off. Disconnect non-essential equipment from the Battery Backup outlets and the turn Back-UPS on. |
F02 On-Battery Output Short | Turn the Back-UPS off. Disconnect all equipment from the Battery Backup outlets and the turn Back-UPS on. Re-connect equipment one item at a time. If the output is tripped again, disconnect the device that caused the error. | |
F03 On-Battery Xcap Overload F04 Clamp Short F05 Charge Error F06 Relay Welding F07 Temperature F09 Internal Error | Errors F03-F09 cannot be corrected by the user, contact SEIT Technical Support for assistance. |
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: