{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to have access to M218 controllers in Machine Expert

NOTE: M218 are obsolete controllers, from v2.2 they stopped being integrated into Machine Expert.

Machine Expert v2.1 or below is needed for the Local Offer Code to work

The M218 controllers are not sold or supported in the US, they are only sold and supported in Asia. So to have access to them you will need to use the Local Offer code that you enter to unlock it from the Machine Expert Installer "Customize" screen: 4Z8X2U2YYJ6PVHWMMW2YDXRUAQ. Here's the step-by-step to do it:

Step 1: Open the Schneider Electric Software installer and select "Modify Installed Software"
Step1

Step 2: Select "Customize version" and click Next
Step2

Step 3:  Click on the configuration dropdown menu on the up-right of your screen and select "Local Offer Code"
Step3

Step 4:  Enter the following code: 4Z8X2U2YYJ6PVHWMMW2YDXRUAQ to unlock the M218
Step4

Step 5: Continue the download process and now you should have the M218 repository in Machine Expert
Step5

Schneider Electric Egypt and North East Africa