Search FAQs
Back-UPS users want a quick and convenient access method to the PowerChute Web UI without the requirement of a username and password.
Issue:
Back-UPS users want a quick and convenient way to access the PowerChute Web UI without requiring a username and password.
Product Line & Device Model:
PowerChute Serial Shutdown
Supported Back-UPS models
Environment:
All supported OS
Cause:
New feature adds
Solution:
PowerChute Serial Shutdown v1.2 + supports Back-UPS users instantly accessing the Web UI via the quick access icon without a username and password combination. This feature benefits users who do not require authenticated or remote access to the Web UI.
Note: Existing PowerChute users (PowerChute Serial Shutdown v1.0) can also remove the username and password requirement by updating it to v1.2.
Back-UPS users want a quick and convenient way to access the PowerChute Web UI without requiring a username and password.
Product Line & Device Model:
PowerChute Serial Shutdown
Supported Back-UPS models
Environment:
All supported OS
Cause:
New feature adds
Solution:
PowerChute Serial Shutdown v1.2 + supports Back-UPS users instantly accessing the Web UI via the quick access icon without a username and password combination. This feature benefits users who do not require authenticated or remote access to the Web UI.
Note: Existing PowerChute users (PowerChute Serial Shutdown v1.0) can also remove the username and password requirement by updating it to v1.2.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: