{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to use temporized start-stop with ATVLogic on ATV320 ?
This video showcases ATV Logic through an example of temporized start-stop with ATV320.
ATV Logic is reachable using SoMove FDT with ATV320 DTM
You can download the latest version of SoMove FDT and ATV320 DTM


🔔 VIDEO Timestamps :
0:06 - Introduction
1:21 - Program with ATV Logic
5:30 - Program explanation
6:48 - Add personalized settings in My Menu
7:49 - Check the program and transfer it to the drive
9:25 - Run the program
9:55 - Operational mode

➡️ For more information see:
• ATV320 - ATV Logic manual NVE71954 (English), NVE71955 (French), NVE71957 (German), NVE71959 (Spanish), NVE71958 (Italian), NVE71960 (Chinese)
Or press "F1" when you are inside the ATV Logic zone in the ATV320 DTM

• ATV320 Programming manual NVE41295 (English), NVE41296 (French), NVE41297 ​​​​​​​(German), NVE41298 (Spanish), NVE41299 ​​​​​​​(Italian), NVE41300 (Chinese)

Schneider Electric Egypt and North East Africa