{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
My UPS shows EPO Activated when the system enable switch is toggled
Issue:
Smart-UPS Ultra 5-10kva displays "EPO Activated" when toggling the system enable switch

Product Line:
Smart-UPS Ultra 5-10kva models: SRTL5KRM2UI, SRTL5KRM2UT, SRTL8KRM4UI, SRTL8KRM4UT, SRTL10KRM4UI, SRTL10KRM4UT

Cause:
This is normal behavior from the UPS.  When the System Enable switch is toggled on the back of the UPS, "EPO Activated" alarm will show.

img1

Resolution:
Please press OK (checkmark) to clear the EPO alarm.

In order to properly perform a Logic Reset or Braindead on this UPS, please follow FAQ000267847.

Schneider Electric Egypt and North East Africa