{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
New DCE Basic and Standard appliances released in 2024 do not support older versions of Data Center Expert.

Issue:
New DCE Basic and Standard appliances released in 2024 do not support older versions of Data Center Expert.

Product Line:
EcoStruxure Data Center Expert

Environment:
Any version of Data Center Expert prior to 7.9.2
AP9465
AP9470

Cause:
Starting in 2024, the newest Dell servers used for the Basic and Standard DCE appliances (R250) support "UEFI" but do not support the older "BIOS" boot option.

Please check server model using the Dell Service Tag for verification.

Resolution:
Because of the change in hardware, as of 7.9.2, DCE has been updated to use both the older "BIOS" and newer "UEFI" option when deploying on a new appliance.
Older versions of DCE were not programmed with the "UEFI" option and as such are unable to deploy on a newer appliance that only has that one option.

Schneider Electric recommends that you keep your DCE up to date as if you need to deploy a new appliance to transfer your configuration and have an existing appliance with an older version of DCE, you will not be able to deploy on the R250.
Future versions of the Enterprise AP9475 DCE server may also have similar limitations.

*Please note that this does not affect the virtual machine deployment option of DCE.

Schneider Electric Egypt and North East Africa