{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can't I downgrade the BMXNOE0100 or BMXNOE0110?
This is due to a new NAND Flash hardware component introduced in Product Version (PV) 27 and greater.

If you have a BMXNOE0100 or BMXNOE0110 that is PV27 or greater, the lowest acceptable firmware level for the BMXNOE0100 is v3.50 and the lowest firmware level of the BMXNOE0110 is v6.70.The downgrade procedure will fail if you attempt to downgrade the firmware of the BMXNOE0100 below v3.50 and BMXNOE0110 below v6.70 with a PV27 or greater.

For more information on the BMXNOE0100 and BMXNOE0110, please visit SE.com.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: