Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Easy-UPS Online Registration
Register the Easy UPS with APC by Schneider Electric customer support. This is a one time process required to be done only during initial installation. The Easy UPS output cannot be turned on without successfully completing registration process. After successful completion of the registration process, the Easy UPS will function normally.
- When the Easy UPS is started up for the first time after installation, the display screen will display 3 numeric digits, “ON LINE”, “ON BATT”, “BYPASS” and “ALARM” symbols on the display get illuminated. All other symbols are not illuminated.
- Call APC by Schneider Electric Customer Support to obtain the 3 digit Personal Identification Number (PIN).
- Press the ENTER button to enter the 3 digit PIN given by APC by Schneider Electric Customer Support. When the ENTER button is pressed, all the 3 displayed digits change to ‘0’ and the first digit flashes every 1 second. Use the UP ARROW button to increment the flashing digit or the DOWN ARROW button to decrement the flashing digit till the first digit of the PIN is displayed. Press the ENTER button to accept the flashing digit and move to enter the second digit of the PIN. Repeat this process till all the 3 digits of the PIN are entered.
- After successful entry of the PIN, a long beep will be heard and the home screen is displayed on the Easy UPS.
- If the authentication of the PIN fails, then a new 3 digit number is displayed and steps 2 to 4 have to be repeated.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Product:
Explore more
Product: