{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the thermal / heat dissipation (BTU/h) of the XB005XPDR?

Issue:

What is the thermal / heat dissipation (BTU/h) of the XB005XPDR?

Product Line:

Easy UPS battery Module XB005XPDR

Environment:

All Serial Numbers

Cause:

Customers are asking why there is no available thermal / heat dissipation rating for the XB005XPDR in the tech specs

Resolution:

There is NO thermal / heat dissipation for the XB005XPDR. The unit does not have loses since this is a DC to DC battery charging system; the heat dissipation is negligible since there are no losses due to conversion.

Thermal dissipation will vary and would depend on internal resistance of batteries so if the batteries are kept on float voltage, there is less than 1 watt of heat generated as the batteries age and during charge and recharge cycle there may be losses thru internal resistance of battery which would be higher as the battery ages.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: