Issue:
Uploading a project from an HMI using Vijeo Designer programming software.
Product Line:
Vijeo Designer, HMIGTO, HMISTU, HMIGTU, HMISTO5, XBTGT
Resolution:
1) Launch Vijeo Designer.
2) Right-click on Vijeo Manager and select "Upload Editor Project".
3) Select the method by which you wish to upload the project. You can upload via Ethernet, Serial, or USB. If you wish to upload via Ethernet, enter the IP address of the HMI.
Publicado para:Schneider Electric España