Hae usein kysyttyjä kysymyksiä
What is the Mean Time Between Failure (MTBF) for the Modicon M340 CPU's?
The following table indicates the calculated MTBF for M340 CPU's. The values are in hours and years for continuous usage at 30 degrees C / 86 degrees F.
Reference number | Continuous hours @ 30 degrees C | Continuous years @ 30 degrees C |
BMXP341000 | 413347 | 47 |
BMXP342010 | 389418 | 44 |
BMXP342020 | 391864 | 45 |
BMXP342030 | 384868 | 44 |
Legacy KB System (APS) Data: RESL186926 V1.0, Originally authored by DaSo on 07/11/2007, Last Edited by DaSo on 07/11/2007
Related ranges: Modicon M340
Julkaistu:Schneider Electric Suomi
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: