Hae usein kysyttyjä kysymyksiä
Unable to select device in Modbus Import Module when connecting to an external Modbus master and downstream slave using VIP
Issue
In the VIP, the Modbus Import Modules properties shows "Not_a_valid_device" when trying to select the Device Name.
Product Line
ION meters
Environment
ION Enterprise 5.5
Struxureware Power Monitoring 7.0(SPM)
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Cause
'MI1 Device Name' shows, "Not_a_valid_device" because no modification of the Virtual Processor Setup tool was done.
Resolution
The ION Virtual Processor Setup must be configured to include the desired Modbus network. The following procedure explains how to add the Modbus network in the ION Virtual Processor Setup:
- Access the ION Virtual Processor Setup via Management Console > Tools.
- Expand the Modbus Network item.
- Add a new Master site.
- Expand the Master site and add a Device
See attachment for more information.
Julkaistu:Schneider Electric Suomi
Liitteet
Lue lisää
Tuote:
Lue lisää
Tuote: