Hae usein kysyttyjä kysymyksiä
Can a ION7300 meter with the Profibus option use other protocols?
Issue
User needs to know if an ION7300 with the Profibus option can use other protocols in addition to Profibus
Product Line
ION7300
Environment
Protocols
Resolution
Yes, the ION7300 meter with the Profibus option is also equipped with RS-485 port COM1. COM1 can be used to communicate using Modbus RTU or the ION protocol.