Hae usein kysyttyjä kysymyksiä
Which maximum current can the tap off units withstand?
For tap off unit reference n°04151 => In: 35A (6²) et 45A (10²) at 40°C
For tap off unit reference N°04152 => In: 55A (16²) at 40°C
The current is limited by the cage terminal not by the cable cross section.
Legacy KB System (APS) Data: RESL196279 V2.0, Originally authored by SeOs on 12/31/2008, Last Edited by GwPo on 06/25/2010
Related ranges: Prisma Plus