Hae usein kysyttyjä kysymyksiä
What is the default directory for ICD files installed with the SFT common library?
Issue
Need the default ICD file for a SEPAM relay.
Product Line
CET850
ICE61850
Resolution
The default directory is as follows:
Install drive (Typically C) > Program Files (X86) (Only X86 if installed on a 64-bit operating system) > Schneider > SFTCommon > IEC61850 > Edition_1 > ICD
This directory contains all of the ICD files that CET850 contains.
Julkaistu:Schneider Electric Suomi
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: