Question:
As for the X80 DDO module, ‘Reactivate’ has the options ‘Programmed’ or ‘Automatic’ – If I select ‘automatic’ will it reset the overload?
Answer:
No, ‘Automatic’ means if the outputs are cut off(physically), the rearmament is performed by the module each 10 second.
As for the X80 DDO module, ‘Reactivate’ has the options ‘Programmed’ or ‘Automatic’ – If I select ‘automatic’ will it reset the overload?
Answer:
No, ‘Automatic’ means if the outputs are cut off(physically), the rearmament is performed by the module each 10 second.
Julkaistu:Schneider Electric Suomi