RemoteConnect to SCADAPAck x70 communication protocol and communication link selection
The PC Communication defines the communication protocol and communication link used for communication between a personal computer (PC) running RemoteConnect software and a target controller, SCADAPack 47x or SCADAPAck 57x. To change communication settings:
1. Open RemoteConnect software
2. Open project that has to be downloaded to SCADAPack x70
3. Click the "PC Communication Settings - DNP3 CommDTM
4. Click the "Offline - PC Communication Settings" tab
5. In the "Connection Type" box select PC Communication Type/Protocol
6. In the box "Serial Communication Settings" configure communication port
7. Click the Apply button Remote Connect screen

Schneider Electric Suomi

Lue lisää
Tuotesarja:
Artikkelit, joista voi olla apua
Lue lisää
Tuotesarja: