Hae usein kysyttyjä kysymyksiä
What are the supported features of the Safety Logic Controller memory key?
Issue:
Supported features of the Safety Logic Controller memory key
Product Line:
TM5
Resolution:
The memory key on the Safety Logic Controller supports the following features:
Supported features of the Safety Logic Controller memory key
Product Line:
TM5
Resolution:
The memory key on the Safety Logic Controller supports the following features:
- holds the safety-related application that is loaded at boot-up.
- storage medium for the application, configuration, and parameters.
- application transfer of safety-related functions to another Safety Logic Controller
Julkaistu:Schneider Electric Suomi
Lue lisää
Tuotesarja:
Lue lisää
Tuotesarja: