Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Schneider Electric launches the first APC Back-UPS™ Pro Gaming designed specifically for gamers

Hong Kong

01/03/2024

Download PDF
  • The APC Back-UPS Pro Gaming keeps gamers protected, connected and in the game, protecting gaming gear against harmful power irregularities

Hong Kong, March 1, 2024 – Schneider Electric, the leader in the digital transformation of energy 28ushwtbqz-phpvnzp0omanagement and automation, introduces the APC Back-UPS Pro Gaming, its first uninterruptible power supply (UPS) designed specifically for gamers. Received the prestigious iF Design award, the APC Back-UPS Pro Gaming features a patented Reactor Circle. When the UPS is in power mode, the circular LED ring indicates the backup power supply's remaining runtime and power level. The sine wave power ensures a stable and high-quality voltage for gaming professionals at critical moments, ensuring an uninterrupted gaming experience. The APC Back-UPS Pro Gaming also boasts efficient power capacity with an output of up to 2200VA / 1320W, allowing gamers to immerse themselves in high-performance games and enjoy exceptional gaming performance.

In the thriving gaming industry in Hong Kong, gamers seek an unparalleled gaming experience. However, the uncertainty of power outages poses a significant threat, leading to frustration and loss of progress. Catering to the unique gaming requirements of e-sports players and gamers, Schneider Electric introduces the first APC Back-UPS Pro Gaming, a revolutionary gaming accessory specifically designed with gamers in mind, delivering uninterrupted power protection as well as ensuring gamers can enjoy continuous gaming experiences even with unpredictable power outages.

By incorporating the APC Back-UPS Pro Gaming into gaming setups, gamers can enjoy a worry-free gaming experience:

  • Protected: The gaming battery backup protects valuable gaming systems from different power disruptions and damage.
  • Connected: Once the gaming system has been properly shut down, the UPS continues to supply power to routers and/or modems, ensuring that equipment remains connected.
  • In the Game: In the event of an interruption or loss of power during gameplay, the backup power supply gives players enough time to save their progress or complete the game, preventing dropped games and resulting penalties.

 

Features of the APC Back-UPS Pro Gaming:

Patented Reactor Circle

Provides the status of remaining usage
time and power level of the backup
power supply, while flashing warning
lights indicate abnormal voltage. The
circular LED ring is equipped with 12
RGB light colors, allowing gamers to
customize the colors to match their
gaming equipment.

gcjvaewycp-phpt1uuor

Quality Sine Wave Power

Delivers stable and smooth output
voltage that is essential for sensitive
gaming electronics. It effectively protects
devices against power irregularities and
potential glitches during power outages,
prolonging the lifespan of gaming equipment.

1fx8f2lz6z-phpel9xc9

High Power Capacity

Features a high-power capacity of
2200VA/1320W, accommodating gaming
equipment with high-performance requirements.
This includes personal gaming computers
with powerful graphics cards, ensuring a
smooth visual experience at high frame rate.

4nr2h4w64x-phpzvzech

 

"With the huge gaming community in Hong Kong and the growing demand for advanced, immersive gaming experiences, power outages can result in significant losses for gamers, especially during player-versus-player (PvP) ranked matches,” said Steven Lee, Director of Secure Power, Power System & Industrial Automation, Schneider Electric Hong Kong. “The APC Back-UPS Pro Gaming provides gamers with a reliable solution to ensure their high-performance gaming equipment is not interrupted by power outages, providing optimal protection and enhancing the overall gaming experience.”

From March 1 to April 30, 2024, customers who purchase the APC Back-UPS Pro Gaming from designated retailers will receive a complimentary Schneider Electric extension socket, available on a first-come, first-served basis while stocks last. Click here to find out where to buy.

 

Appendix – Product Information of the APC Back-UPS Pro Gaming

APC Back-UPS Pro Gaming

qbmea4tlwy-phpoiibrw

411bshon1y-phpgoiddr

Midnight

BGM2200B-UK

Arctic

BGM2200-UK

   Size

  • H:11.5in * W:4.1in * D:16.1in

   Unit Weight

  • 27.16lbs / 12.32kg

   Power Capacity

  • 2200VA / 1320W

   Output Connections

  • 4 (2 IEC & 2 UK)

   Wave Form

  • Sine Wave

   Protection

  • Surge Energy Rating: 1080 joules
  • Dataline Surge Protection (Gigabit)
  • Input Over Current Protection: 15A circuit breaker

   Color

  • Midnight (BGM2200B-UK)
  • Arctic (BGM2200-UK)

   Warranty

  • UPS: 3 years
  • Battery: 15 months
     

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!