{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the maximum number of fault current operations Ringmaster and GenieEvo will clear?

The number of faults that a circuit breaker can clear will depend on the level of fault current being interrupted.

Ringmaster: -
  • 16kA - the circuit breaker is designed to clear a maximum number of 11 times at 16kA fault current
  • 21kA - the circuit breaker is designed to clear a maximum number 10 times at 21kA fault current

GenieEvo is designed to clear a maximum of 100 faults at 25kA.

The fault current rating of the unit is detailed on the unit rating plate.

Schneider Electric Hong Kong

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: