FAQ Pencarian
What is the Serial Number to use when installing SFT2841?
Product Line
SEPAM Relays
SFT2841
Environment
SEPAM SFT2841 software installation
Resolution
The serial numbers to use while installing the software are:
- For SFT2841 versions 11 and above: 0647740-08
- For SFT2841 versions below 11: 8888888-06