FAQ Pencarian
What is the part number for Vijeo Designer Lite version 1.3?
Issue:
Vijeo Designer Lite part numbers
Product Line:
Vijeo Designer Lite
Resolution:
Below are the new part numbers and descriptions for Vijeo Designer Lite
VJDSNDTMSV13M | Vijeo Designer Lite, Single license Software version V1.3 for developing and implementing an application for XBTN/R/RT on 1 PC. Supplied without cable Cancels and replaces VJDSNDTMSV12M |
VJDSUDTMSV13M | Vijeo Designer Lite, Single license, Matrix XBT download USB cable Software version V1.3 for developing and implementing an application for XBTN/R/RT on 1 PC. Supplied with a USB cable for XBTN/R/RT (XBTZ925+ TSXCUSB485) Cancels and replaces VJDSUDTMSV12M |
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: