FAQ Pencarian
Why do I receive the error "Incompatibility between the dropped module and the last module of segment 1", when trying to add a module following the STBCPS2111 Auxilliary Power Supply?
The reason this error is received is because when a STBCPS2111 Auxilliary Power Supply is added to the segment it has to be followed by a PDM module and then add a compatible IO module.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: