ION8650 meters do not allow the configuration of more than 100 DNP base points from ION Setup
It will actually let you keep adding to the parameter map but when you exit setup assistant it throws this message:
"The following modules are off-line and may indicate an improperly configured feature in the device" as shown below:
When you try to bring the modules online, the following error message is displayed:
"Too many DNP points configured in DSE" as shown below:
Product Line
ION 8650 Meters A, B and C
ION Setup
Environment
ION8650 DNP Static Points
Cause
Unable to configure over a 100 DNP base points on an ION8650s in ION Setup
Resolution
The limitation for DNP base points on ION 8650 meters is 100 as stated below:
This information can be found under the Powerlogic ION8650 DNP 3.0 Device Profile document, which can be downloaded from the link below
http://download.schneider-electric.com/files?p_Reference=70022-0126-00&p_EnDocType=User guide&p_File_Id=27606449&p_File_Name=70022-0126-00.pdf
Diterbitkan untuk: Schneider Electric Indonesia


Perlu bantuan?
Mulai di sini!
Temukan jawaban sekarang. Cari solusi sendiri, atau hubungi salah satu pakar kami.
Hubungi Dukungan
Hubungi tim layanan pelanggan kami untuk mendapatkan informasi lebih lanjut, bantuan teknis, penanganan keluhan, dan lainnya.
Tempat pembelian
Temukan distributor Schneider Electric terdekat di lokasi Anda dengan mudah.
Jelajahi FAQ
Dapatkan jawaban yang Anda butuhkan dengan menelusuri Pertanyaan yang Sering Diajukan (FAQ) berdasarkan topik.
Hubungi Bagian Penjualan
Silakan kirimkan pertanyaan terkait penjualan secara online dan pakar kami akan menghubungi Anda.