FAQ Pencarian
How to identify oversized historical granules in ClearSCADA
Issue
ClearSCADA is designed to support maximum 4 historic updates per minute per point. Exceeding the limit will create historic files larger than 1.3MB and might affect the performance of the system. It is recommended to remove oversized historic files (granules) and to analyze relevant points historic storage rate.
Product Line
ClearSCADA (EcoStruxure™ Geo SCADA Expert)
Environment
Windows OSes
Resolution
Oversized historic files can be identified using SQL Query (embedded list or in the Query Pad) and command line.
Both ways are suitable, however command-line could be modified to move the identified granules to another location in addition to the search routine.
Code can be copied to any Simple Text Editor and saved with .cmd extension.
1. Check the location of the Historic Data (in the Server Administration tool) and copy the path.
2. Create a Folder and create a text file with the following content:
PAUSE
3. Replace the text in <> accordingly.
4. Save the file with .cmd extension.
5. Execute the command line file under the Administrator permissions.